Cancel
Showing results for 
Search instead for 
Did you mean: 

Add-In Manager

Not applicable

Can I use Add-In Manager with Solid Edge 2D and how?
Thanks
Hendrik Smit
New e-mail address: hendrik@sisonkehydraulics.com
3 REPLIES

Re: Add-In Manager

Not applicable
Hendrik,
The Add-In Manager command should be disabled for the free Solid Edge 2D
Drafting. The applications interface is disabled. you cannot write your own
macros to drive the product.
Regards,
Rick B.

Re: Add-In Manager

Not applicable

"Ricky Black" wrote:
>Hendrik,
>The Add-In Manager command should be disabled for the free Solid Edge 2D
>Drafting. The applications interface is disabled. you cannot write your own
>
>macros to drive the product.
>
>Regards,
>Rick B.
>
>Ricky,

The Add-In Manager is disabled.
Is it enabled in free2d maintenance?
Also is their a Mechanical Structure available like in Autocad Mechanical?
Or Layers and sub-layers ie:
Barrel Assy
Barrel
Base
Clevis
Thanks for the quick response.
Regards
Hendrik


Re: Add-In Manager

Not applicable
Hendrik,
The applications interface is enabled in the maintenance version of Solid
Edge 2D Drafting. This license enables the Drafting part of the overall
Solid Edge API. You cannot create or manipulate 3D derived objects such as
drawing views through the API with this license. The 3D derived content is
disabled.
There is no assembly type structure in 2D drafting.
Regards,
Rick B.