Cancel
Showing results for 
Search instead for 
Did you mean: 

Add a hem

Honored Contributor
Honored Contributor

How can I fold an existing piece of sheet metal 180 deg (or a hem).

 

The existing hem command add's material. I'm looking to bend existing material.

 

If I use a flange or bend command, things don't work right as I approach 180 deg.

2 REPLIES

Re: Add a hem

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Is this what you are looking for?

 

 

Cheers

Mark

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

Re: Add a hem

Honored Contributor
Honored Contributor

I figured it out. I need to use the add bend command with R=0 and Ang=0.

 

Then I can create a hem that does not have straight sides.