Cancel
Showing results for 
Search instead for 
Did you mean: 

Add a plus plus tolerance to a dimension

N/A

Hep
Is it possibel to add a plus plus tolerance to a dimension.
I can only find plus minus……
Regards
Lars
2 REPLIES

Re: Add a plus plus tolerance to a dimension

N/A
Just use the plus/minus tolerance option. SE will only show a plus
tolerance if the minus tolerance field is left blank/0 (or vice versa).
--
Ken
http://grundey.blogspot.com

"Lars Ulrich" wrote in message
news:492fd242$1@bbsnotes.ugs.com...
>
> Hep
> Is it possibel to add a plus plus tolerance to a dimension.
> I can only find plus minus..
> Regards
> Lars
>

Re: Add a plus plus tolerance to a dimension

N/A

"Lars Ulrich" wrote:
>
>Hep
>Is it possibel to add a plus plus tolerance to a dimension.
>I can only find plus minus……
>Regards
>Lars
>

You just type a plus sign in front of the value in the minus box. the tolerance
on the drawing will then show i.e. +0,5 +0,25.
Hope this was what you wanted.
Torleif
TorleifS