Cancel
Showing results for 
Search instead for 
Did you mean: 

Add colour to parts list cells

Valued Contributor
Valued Contributor

is there a way to colour cells of a parts list. like you can do in Excel.

Regards,

MagRiz
(ST9 User Est 01.18)
3 REPLIES 3

Re: Add colour to parts list cells

Gears Phenom Gears Phenom
Gears Phenom
Hi,

There is no way for this.

BR,
Imics
http://solidedgest.wordpress.com/

Re: Add colour to parts list cells

Gears Phenom Gears Phenom
Gears Phenom

@MagRiz wrote:

is there a way to colour cells of a parts list. like you can do in Excel.


There is not a direct option to do it.

 

Once I had the needing to color some cells and what i have done is:

- Draw a rectangle same color of the table grid color

- Fill the rectangle in solid color i want to put in cell

- Move and size the rectangle same dimension and position of the cells to color

- Move the rectangle to background

 

This is just a workoaround, it is time consuming and not automaticcaly updates if the table changes.

So if it is just for one shoot you can do it, but not for everyday works in that case I would fill an ER

Re: Add colour to parts list cells

Valued Contributor
Valued Contributor

@Fiorini Smiley Sad

 

i have to colour this in with my felt tip and scan it..

Regards,

MagRiz
(ST9 User Est 01.18)