Add plane to tube

Builder
Builder

How do I add a reference plane to the centre of a tube, I want a plane creating on the centre line of the tube to run the length of the tube

 

Thanks

6 REPLIES

Re: Add plane to tube

Pioneer
Pioneer

Will plane 'By 3 Points' and setting Keypoints to Silhouette achieve what you need?

585 ST9 Win 7

Re: Add plane to tube

Phenom
Phenom

You can add a parallel reference plane to one of the standard planes passing though the center of the tube. On the Command bar, pick the center point option from the drop-down.

 

2016042701.jpg

Re: Add plane to tube

Builder
Builder

There a several tubes, the tube I want to add a plane to does not have the reference plane, how do I add to this tube ?

Re: Add plane to tube

Esteemed Contributor
Esteemed Contributor

@agoodwin, Pictures, videos, or attached models are helpful in cases like this.

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200

Re: Add plane to tube

Phenom
Phenom

A couple of ways I can think of -

If the ends are perpendicular to the axis, create a plane on the end, then a plane at 90° to that one.

Tangent plane on the cylinder, then a parallel plane offset to centre of cylinder (in ordered) or just move it if in sync (you can also rotate it in sync)

HP Z420 16GB RAM
Quadro K4000
ST10 MP3 on Windows 10 Pro 64.

Re: Add plane to tube

Honored Contributor
Honored Contributor

I'm not sure of your situation, but I would take a step back and ask, how was the tube created? If it's a sync part, the origin can be moved so that an axis of the origin can be your center line. If the part is ordered, it would need to be created on the center line of the tube.

 

In general, I would try to get the center of the tube on the center of the coordinate system of that tube part. Then the coordinate system becomes the axis you desire.

 

If your tubes are already mated using it's own coordinate system, then this could cause problems.