Cancel
Showing results for 
Search instead for 
Did you mean: 

Adding custom symbols to Callout dialog box

Genius
Genius

Is there a way to add custom symbols to the Callout Dialog box?

 

My company has non-standard callouts that are used on a few select dimensions for incoming inspection purposes, these are not going to change to anything else.

 

Symbol gets placed adjecent to relevant dimension. My issue is that when I have these on drawing and the dimension gets moved or view gets moved, the symbol does not get relocated. I attached a screen capture of a drawing that has some on it. The 'M' in a diamond shape is on this drawing. All other symbols are in a diamond shape, others have different letters. Lower left side of drawing has a note indicating meaning and inspection requirements of each.

 

Gary Dinges | Mechanical Design Engineer II | Probes & New Product Development Emerson Climate Technologies | Therm-O-Disc, Inc.| 1320 South Main Street | Mansfield | OH | 44907 | USA T +1 419 525 8554 gary.dinges@emerson.com

2 REPLIES 2
Highlighted

Re: Adding custom symbols to Callout dialog box

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Why not use a diamond balloon shape with "M" inside linked to the dim? It will move with the dim and/or view.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Adding custom symbols to Callout dialog box

Genius
Genius

That works !!

 

Thank You,

 

Gary