Cancel
Showing results for 
Search instead for 
Did you mean: 

Adding dimensioning to detailed view

Builder
Builder

I have a detail drawing view that I am trying to add dimensions to however I am unable to add any dimensions at all to the view. I have updated the view but this does not allow me to add dimensions. Please tell me what is wrong here and how to do this. Thank you

11 REPLIES 11

Re: Adding dimensioning to detailed view

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

What happens when you start a command, say the Smart Dimension, pick an object in the detail view and click to place the dimension ?

Re: Adding dimensioning to detailed view

Builder
Builder

Nothing happens at all, the detailed view will not highlight or allow me to enter the dimension command and place down a smart dimension or any other type of dimension

Re: Adding dimensioning to detailed view

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What happens when you generate another view?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Adding dimensioning to detailed view

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Have you used draft quality views for the original placement. If dimensioning was not enabled, then you will not be able to dimension any other views derived from it.

 

Shane

Shane Murray
SE2019 MP3

Re: Adding dimensioning to detailed view

Phenom
Phenom

In fact tha answer of shane is the right one Smiley Happy

 

If you activate the Draft Quality Views you will not be able to dimension any views.

 

Yasser

 

dimension_quality_views_01.JPG

Re: Adding dimensioning to detailed view

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Perhaps of interest is the apparent fact that if you generate another draft quality view with "activate parts for dimensioning" selected, contrary to what others stated here, other draft quality views become dimensionable. Even if you delete that last view. This method would be in lieu of using "convert to high quality view".

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Adding dimensioning to detailed view

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Thank you! this answer helped me!

Re: Adding dimensioning to detailed view

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bshand

 

Hi @agoodwin

 

 

@bshand is on the right way and pointed out a good fact.

Dimensioning of "Draft Quality Views" and "High Quality Views" is the issue.

But - as there always is a but - the only point is the activation of certain parts to allow to use them (or their edges) for dimensioning.

 

Just use the Activate Part Button on Home Ribbon Bar to activate any part at any time!

After doing so, You also can - without the need of creating a new view - add any dimension to those parts.

Even in the detail view

 

 

20180418_1913.png

regards
Wolfgang

Re: Adding dimensioning to detailed view

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad, Man! I don't even remember writing that. It has been over 2 years though. And you made the process even simpler.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200