Cancel
Showing results for 
Search instead for 
Did you mean: 

Adding options to property manager pull down.

Experimenter
Experimenter

How can I add more options to my pull down list under property manager?  Like selecting materials in property manger... but I have a column that is for the finish of materials.  Right now the options are gold, nickel, copper and black oxide (I added the black oxide as a default)  But I dont know how to add other finishes....so I dont have to type it in each time.

1 REPLY 1

Depends on whether you are working Managed or not.  If yo...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Depends on whether you are working Managed or not.  If you are working Managed, this is controlled by the data management system.  If you are not, then you will be looking for the Propseed.txt file to populate all list boxes except for the Material property.  In ST6, this should be in your Preferences folder.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com