Cancel
Showing results for 
Search instead for 
Did you mean: 

Adding renders in queue in Keyshot?

Legend
Legend

Hi there,

 

is it possible to queue renders in Keyshot 5? I can see there is an "add to queue" button inside Render toolbar, but it is greyed out. I'd like to leave the computer render several different scenes after I leave the office.

 

Thanks

1 REPLY

Re: Adding renders in queue in Keyshot?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There are several packages of Keyshot and I believe that the version included with SE is Keyshot HD.  It is the least featured of all the packages and lacks the Render Queue feature.  If that is something you wish to have, you would have to purchase an upgraded package from Keyshot to get it.  Here is a link to the package feature comparison page:  https://www.keyshot.com/buy/product-comparison/



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com