Cancel
Showing results for 
Search instead for 
Did you mean: 

Adding standard parts for use with the fastener system

Valued Contributor
Valued Contributor

I'm looking for help/advice prior to adding some custom parts to the standard parts database.  I want to add a range of Nork-lock washers.  My question is about the fastener system in SE.  Do I need to do anything specific to allow the custom parts to be used/recognised by the fastener system?

 

Thanks,

Guy


CAD/CAE Manager
SE2019 MP5
15 REPLIES 15

Betreff: Adding standard parts for use with the fastener system

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Guy_H77

 

 

AFAIR ther must be additional properties defined in the standrad parts library to let parts recognized for fastener system use.

 

But this is done so seldom, that I also first have to search for the appropriate document.

 

But in the meantime just do a search in the standrad parts help pages.

 

 

regards
Wolfgang

Betreff: Adding standard parts for use with the fastener system

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Guy_H77

 

 

when in Standard Parts Administrator and openeing the help (F1) a search for "fasten" bring at least 2 pages explaining the proeprties needed for them.

 

20170525_1049.PNG

regards
Wolfgang

Betreff: Adding standard parts for use with the fastener system

Valued Contributor
Valued Contributor
Thanks Wolfgang. I'll give that a go. We use the SMAP database but I believe it is the same as they provide it for SE.

Cheers,
Guy

CAD/CAE Manager
SE2019 MP5

Betreff: Adding standard parts for use with the fastener system

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Guy_H77

 

 

Yes I think this is absolutely correct.

The Solid Edge Standard Parts DB IMHO is a subset of the big SMAP tool

Theer it should be a lot easier to add new parts to Your DB

regards
Wolfgang

Betreff: Adding standard parts for use with the fastener system

Valued Contributor
Valued Contributor
@hawcad

Strangely there is no mention in the SMAP database administrator help files about the fastener system in SE. I'll investigate further......

Thanks,
Guy

CAD/CAE Manager
SE2019 MP5

Betreff: Adding standard parts for use with the fastener system

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Guy_H77

 

do You have a installation with the normal Standard Parts Database installed.

If not I think You can do it on YOur computer what will take a couple of minutes and then YOu will have the help pages for it.

 

regards
Wolfgang

Betreff: Adding standard parts for use with the fastener system

Valued Contributor
Valued Contributor

Found the info.  Seems it should be easy enough....

 

 

Step 1

Select 'Add from manual data entry' and click on 'Next'.

 

Step 2

In this step you should select the parts you want to register as customer standard parts. You can add documents from a specified path in bulk (Add Path) or add particular files (Add Files). You can even remove files from the list (Files to Add) via the 'Remove selected' button.

 

Step 3

Settings in this step are optional. If you want your custom part to be used as a fitting (or tube) by Solid Edge Piping, you can check 'Add to Piping' option and set a number of coordinate systems pairs. To create a custom part to be used in Fastener Systems, check 'Add to Fastener System' and select appropriate Fastener type (bolt, screw, washer or nut).

 


CAD/CAE Manager
SE2019 MP5

Betreff: Adding standard parts for use with the fastener system

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Guy_H77

 

 

I just searched for the help file of Standrad Parts Admin and share it here to You

 

 

regards
Wolfgang

Betreff: Adding standard parts for use with the fastener system

Valued Contributor
Valued Contributor

thanks Wolfgang!


CAD/CAE Manager
SE2019 MP5