Showing results for 
Search instead for 
Did you mean: 

Additional Frame Profiles?


Greetings experts!


My installation of Solid Edge ST7 only has a handfull of frame profiles to chose from. 

See attached picture of square tubing selections available.  

Is there a more complete library that is available to download? 

Or will I have to manually create standard profiles? 




2015-12-10 09_17_02-Frame.png



Betreff: Additional Frame Profiles?

Esteemed Contributor
Esteemed Contributor





if You have a SE Classic or Premiuim, You also have the Standard Parts Library, and there You can find a lot of standard profiles.


If not, then You have to creta them by Yourself, but that is a very easy task.


Use sequentiel parts, with one single extrusion showing Your profile with a certain length (e.g. 100 mm)


That's all.




Re: Additional Frame Profiles?

Honored Contributor
Honored Contributor

I ended up creating my own profiles because I use the fundamental version of SE. The extra cost/year was not worth the cost of creating the 50 profiles I actually use. For my application (sheet metal fabrication) there was no other advantage to the upgrade.


I attached a file with what I have created for frame cross sections