Cancel
Showing results for 
Search instead for 
Did you mean: 

Adhesive CAD Symbols

Experimenter
Experimenter

Anyone using Adhesive CAD Symbols in drafts, per ASTM D7447-08?  I'm interested in finding a Solid Edge (ST10) application for the ASTM D7447 adhesive / sealant symbol.

3 REPLIES 3

Re: Adhesive CAD Symbols

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@rdelp Didn't know that existed until now.  Looks like the ASTM weld symbology.  Makes sense...

 

Haven't seen anything for SE though.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Adhesive CAD Symbols

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

A little searching on this standard, which is also new to me, revealed that AutoCad has these symbols. If you have any AutoCad seats perhaps you can swipe the symbols from there and use them in edge as blocks.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200
Highlighted

Re: Adhesive CAD Symbols

Gears Phenom Gears Phenom
Gears Phenom
In my previous employment we did use SE Weld Symbols and then "attached" blocks with the other symbols and data tables to the weld annotation.

Sorry, I no longer have access to those.

____________________________________
--Scott Wertel, P.E.