Cancel
Showing results for 
Search instead for 
Did you mean: 

Adjust Assembly Batch Off??

Valued Contributor
Valued Contributor

Hello.. Edge Users
Questions about adjustable assemblies.
I made several subassemblies into adjustable assemblies.
And saved.
The next time you open, you do not need an adjustable assembly.
Adjustable assemblies applied to multiple subassemblies in batches
Is there a way to disable it?

3 REPLIES

Re: Adjust Assembly Batch Off??

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Are you asking if you can switch multiple assemblies at once between flexible and rigid?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200
Highlighted

Re: Adjust Assembly Batch Off??

Valued Contributor
Valued Contributor

Hello bshand..

After applying the variable assembly to several subassemblies
I am asking how to disable it at once.

Re: Adjust Assembly Batch Off??

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

So you want to switch them back to rigid at once instead of doing it separately on each assembly? All the same assembly or different assemblies?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200