Cancel
Showing results for 
Search instead for 
Did you mean: 

Adjust table margins (to fit more text)

Experimenter
Experimenter

Hello ! Thank you for reading this out,

I'm trying to fit a word in a column without it breaking

(example vs exam

ple)

All I see is two choices.

1- Lower the font size until the word fits without breaking. But then I end up with a word in 0.02 size font.
2- "Adjust text to column width". But then I end up with a really squeezed word.

I realised that I have a lot of space on either side of my word, in other words, a large margin. Is there a way to reduce this margin so the word would fit ? See the attached picture.

The "Rev" at the botton is a text box and fits well. But the "Rev" at the top is really stretched although they have the same font size.

 

Thank you guys!

2 REPLIES 2

Re: Adjust table margins (to fit more text)

Gears Phenom Gears Phenom
Gears Phenom
In the table properties, first page, check the "Horizontal margin" value, you can low it to 0

Re: Adjust table margins (to fit more text)

Experimenter
Experimenter
Wow that was it ! Right here in my face on the first page. I spent a lot of time looking through the Style in "Indents and spacing".

Thank you so much!