Cancel
Showing results for 
Search instead for 
Did you mean: 

Adjust thickness of revolved feature

Experimenter
Experimenter

I created a revolved feature, and the sketch used to define it has a thickness.  I can change the thickness before creating the revolution, but I want to be able to update the thickness after creating the revolution, but it doesn't allow me to.Untitled.pngUntitled.png

1 REPLY

Re: Adjust thickness of revolved feature

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @inyikos,

 

I think, given your design criteria, you might be better served using the "thin-wall" command to control the wall thickness, which is exactly what it is designed for, and is easily editable.

[see my attached example file]

 

 

EDIT: sorry, I had to "ZIP" [compress] the file, as the community seem unable to upload this file type anymore. @KatieKing, can you check this? It said *.PAR was an unsupported file type.

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000