Cancel
Showing results for 
Search instead for 
Did you mean: 

Adjustable part that wont adjust

Phenom
Phenom

This is the second time i come into this problem and I haven't figured out how to solve it.

I do usually import models from supplier, clean them a bit and add the adjustable feature I need to use in my assembly.

 

In this case it's a pump where I want to be able to define the electric box rotation at assembly level.

 

Adjustable part works well if I change the value in part, but it doesn't work at all if try to use it in an assembly.

 

Am I missing something ?

 

Thanks

2 REPLIES

Re: Adjustable part that wont adjust

Phenom
Phenom
For the records, I have inserted a copy of the model in a new one and recreated the adjustable feature and now it works.

I would know a less destructive way to fix it.

Re: Adjustable part that wont adjust

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That's a novel (to me) way (using "rotate faces" in ordered) to solve the problem of grouping the faces in that electrical box and get a dimension variable to adjust. Very nice. I'm glad I downloaded and looked at it.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200