Cancel
Showing results for 
Search instead for 
Did you mean: 

Advance Steel export into Solid Edge?

Legend
Legend

Has anyone exported models from Advance Steel to open in Solid Edge? We are new to this Advance Steel, and when we export, we lose some holes when imported to Solid Edge. Maybe one export extension works better with Solid Edge import?

3 REPLIES 3

Re: Advance Steel export into Solid Edge?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you tried the IFC export?



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com
Highlighted

Re: Advance Steel export into Solid Edge?

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

As @KennyG has mentioned IFC should be working...

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Advance Steel export into Solid Edge?

Legend
Legend

Hi,


As mentioned before, IFC import will do the trick.. but...

 

We did a testrun with Tekla.. a similar program... and in this kind of software "holes"  are not "drilled" into the beam.. its a sort of internal reference, to show a circle on a drawing and to project 3D view of a bolt / nut combination when you look at that connection in 3D...

So when you do a export, there is no hole to export... and you will end up with a lot of beams and plates without holes...   !@#$^%@$^....

 

There is a fundemental difference between solid modellers and those "database" oriented steel frame built software.

 

Succes and kind regards,

 

Jan Bos

Emmen, The Netherlands