Cancel
Showing results for 
Search instead for 
Did you mean: 

After entering activation code status bar loads for days but doesnt complete

Experimenter
Experimenter

I downloaded the 45 day free trial of Solid Edge ST7 a few days ago and when I enter my activation code the status bar that shows its loading and processing my activation continues to load forever but doesn't complete. I left it running to load for 3 days and it still did nothing except say it was processing my activation and that it should only take a few minutes. I am a student and I have work to do. I really need help as soon as possible and any help is greatly appreciated.

1 REPLY

Re: After entering activation code status bar loads for days but doesnt complete

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

"3 DAYS", Yikes!!!...no way I'd have waited longer than 3 minutes, and thats being rather generous for the action being performed. This type of problem points to a corrupt installation file, or incompatible system.

 

If you're a student....why not download the free "Student Edition"?

 

 

 

Aslo to note....Solid Edge ST7 is the first release that is ONLY coded for use in 64bit Windows.

[stay on ST6 if you have a 32bit installation of Windows]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000