Cancel
Showing results for 
Search instead for 
Did you mean: 

Air Vacuum Pressure Test

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I would like to know if SE has the tools to equate vacuum and air pressure.

As shown on this video the vacuum port is the center, air pressure is the outer ports.

 

http://screencast.com/t/NaDbHgbB

 

Thank You

Greg

2 REPLIES 2

Greg, Can you not calculate this by measuring the cross...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Greg,

 

Can you not calculate this by measuring the cross sectional "area" of each apperture?

But, as for Solid Edge doing this, I'm not sure if the limited "Solid Edge Simulation" has this functionality, it may well be a tool set of the more advanced FEA application.

 

Some more info here....

http://www.plm.automation.siemens.com/en_us/products/velocity/solidedge/overview/add_on_apps/simulat...

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Hi,   I suggest to use Goal seeking command in sketch. Wh...

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

I suggest to use Goal seeking command in sketch. What you want to do is a bit complex, but I hope this will help:

 

BR,

Imi

Imics
http://solidedgest.wordpress.com/