Cancel
Showing results for 
Search instead for 
Did you mean: 

Align an axis with a face (use an offset)

Valued Contributor
Valued Contributor

Hi,

 

Is connect the only way to create a constraint between an axis of a cylindrical part and the face of a mating part?  

 

Thanks,

Guy


CAD/CAE Manager
ST8 MP12
1 REPLY

Re: Align an axis with a face (use an offset)

Genius
Genius
from what i have used yes connect is best option. Connect with a specified number will offset an axis from a face. Can you post a screenshot of what you are trying to do? Center plane? However you would need 2 faces for second selection set.
Cory M
Solid Edge ST10
ST10 Cert