Cancel
Showing results for 
Search instead for 
Did you mean: 

All around symbol on a radii dimensionsimilar to callout??

Genius
Genius

Is there a way to add an All Around symbol as part of Radius dimension? Similar to the one the callout dialog has?

 

Picture attached.

 

Gary Dinges | Mechanical Design Engineer II | Probes & New Product Development Emerson Commercial & Residential Solutions | Therm-O-Disc, Inc.| 1320 South Main Street | Mansfield | OH | 44907 | USA T +1 419 525 8554 gary.dinges@emerson.com

 

10 REPLIES 10

Re: All around symbol on a radii dimensionsimilar to callout??

Legend
Legend
Looks like no, at least I can't find one on ST10-MP3, interestingly though in the properties dialog box on the terminator and symbol tab the last section is All-Around Symbol, with a size spec box.

Re: All around symbol on a radii dimensionsimilar to callout??

Siemens Phenom Siemens Phenom
Siemens Phenom

To the best of my knowledge the "All Around Symbol" is a GD&T symbol using for tolerancing and welding.  It is not a recognized symbol for dimensional drafting. 

Re: All around symbol on a radii dimensionsimilar to callout??

Honored Contributor
Honored Contributor

Add a circle to the arrow manually. Old school I know.

Re: All around symbol on a radii dimensionsimilar to callout??

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Or add a callout with the R value typed in.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: All around symbol on a radii dimensionsimilar to callout??

Genius
Genius

12gage:

Tried circle idea, about 1st thing. Can't snap to the leader line, so I can't anchor circle.

I did a call out on it.

Probably going to Hades for doing that.

 

Gary

 

Re: All around symbol on a radii dimensionsimilar to callout??

Legend
Legend

I tried to find a callout, but had not luck. There, you can use the all around symbol. I wonder if there's a formula for radius that you can add to the callouts.

Re: All around symbol on a radii dimensionsimilar to callout??

Experimenter
Experimenter

For UG NX:

Insert Annotation Balloon; leave Text blank, change Size to something small (2.0), Origin, Specify Location, Associative {so circle remains the same (-X) distance to the left as the leader jog, of the Note or Annotation getting the symbol}.

Re: All around symbol on a radii dimensionsimilar to callout??

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Quantum_1  schrieb:

Insert Annotation Balloon; leave Text blank, change Size to something small (2.0), Origin, Specify Location, Associative {so circle remains the same (-X) distance to the left as the leader jog, of the Note or Annotation getting the symbol}.


 

Hi @Quantum_1

 

 

do I miss someting?

Which Solid Edge Version are You using here?

 

regards
Wolfgang

Re: All around symbol on a radii dimensionsimilar to callout??

Experimenter
Experimenter

Hi Wolfgang,

I mistakenly posted this on Solid Edge when I should have posted on NX.

Thanks for the reply,

Chris