Cancel
Showing results for 
Search instead for 
Did you mean: 

All parts of a solid edge assembly missing when opening the assembly

Pioneer
Pioneer

Hi,

 

I was trying to open a solid edge assembly and all the parts in it don't show up and they are also missing from the cache folder. Is there a way to fix this without opening each and every part of the assembly? 

 

Thanks.

Dag

6 REPLIES 6

Betreff: All parts of a solid edge assembly missing when opening the assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Dag

 

 

 

 

have You changed anything regarding this assembly?

 

Have You moved or renamed it, have You changed the folder structure etc. from any of them?

 

Are there any error messages regarding a missing part?

 

Can You see them in pathfinder and Your parts are only hidden?

 

 

regards
Wolfgang

Re: All parts of a solid edge assembly missing when opening the assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

How long since your last reboot? You're using Insight or TC?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: All parts of a solid edge assembly missing when opening the assembly

Pioneer
Pioneer
I have not changed anything. I can see the assembly tree but the parts have question marks on them. Whenever I open the assembly it gives me the message saying "the following parts are missing" and shows the list of all missing parts. I have the assembly and all the parts created and statused in teamcenter so there is no possibility of them being deleted. The parts are not hidden either. I can see them in path finder.

Re: All parts of a solid edge assembly missing when opening the assembly

Pioneer
Pioneer
I just rebooted my pc today. I am using teamcenter.

Re: All parts of a solid edge assembly missing when opening the assembly

Honored Contributor
Honored Contributor

Do you have the parts that are not showing up open in another instance of SE?

 

Each file can only be opened up once by each user.

Re: All parts of a solid edge assembly missing when opening the assembly

Pioneer
Pioneer

I don't have them open anywhere. For some reason the parts in the assembly are not being populated in my cache folder. Usually when I open an assembly the cache folder would be populated both with the assembly and part files.