Cancel
Showing results for 
Search instead for 
Did you mean: 

Alternate Assembly Icon is blank

Phenom
Phenom

Hi,

 

I decide to start a new inquiry.

 

Could you please to tell me why in some assemblies the New Alternation Icon is blank ?

 

I spotted that in a few ASYs.

 

Thank you,

 

ArekAlternate ASY options Issue.png


Production: SE ST10 MP8
;
3 REPLIES

Re: Alternate Assembly Icon is blank

Legend
Legend

Hi,

 

if you have mirrored parts, alternate assemblies is greyed out.

Re: Alternate Assembly Icon is blank

Siemens Phenom Siemens Phenom
Siemens Phenom

It is disabled for various reasons:

  • you are editing the assembly in-place
  • the assembly has been edit-opened (selecting Open on the context menu for a subassembly)
  • you are in the ERA environment
  • you are in the XpresRoute environment

Greg

 

Re: Alternate Assembly Icon is blank

Genius
Genius

To expand upon Greg's response:

When you open alternate/Family of assemblies from a drawing or a higher level assembly, it will only open that instance or child member and will not allow you to edit any or all other members.  If you want to edit all members close the file and reopen it via the open dialog box.  Now these icons should be available.

Brian Fritz
Solid Edge Certified Professional
ST10 latest MP