Cancel
Showing results for 
Search instead for 
Did you mean: 

An alternative for solidworks QuickPress and LogoPress

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I have a client that uses Solid Edge and so far he is satisfied with the new software . Lately however he has been asking whether is there any other alternative offering of SolidWorks QuickPress & LogoPress 

 

("I guess he is not satisfied with the create blank function in Solid Edge and wants more flexibility that QuickPress & LogoPress can provide")

 

So folks, any ideas?

1 REPLY

Re: An alternative for solidworks QuickPress and LogoPress

Phenom
Phenom

Depends on the level of functionality the customer is wanting. If the customer is after full blown progressive die design with animation then I would recommend that they look at NX Progressive Die Design seat and use SE the rest of the design/engineering. 

 

Can't beat the support, functionality, simulation and analysis functions built into this module.