Cancel
Showing results for 
Search instead for 
Did you mean: 

Angle dimensions in Cut list incorrect.

Experimenter
Experimenter

I am extremely new to the platform so please excuse me if this is a dumb question. I have noticed that some of my cut angles in my parts lists are showing incorrect angle measurements. 

 

Item 4 on the cut lists should show about 30* on CUT 1 and 60* on CUT 2. Item 5 should show around 45* on both cuts. I am somewhat confused because the other line items are showing the correct cut measurements. 

Cut list.PNG

-Brock
SE2019
2 REPLIES

Betreff: Angle dimensions in Cut list incorrect.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @_CF_

 

 

this is an old fashioned and wellknown issue.

 

The Miter Cut Angles are only calculated and shown for corner connected frames of the same frame group.

The pos numbers You mentioned are extra frames and trimmed back to the existing frame components.

And these mitter angles are not shown.

 

 

regards
Wolfgang

Betreff: Angle dimensions in Cut list incorrect.

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi,
really? Nothing has changed with this issue? i can not believe that simens allows something like that.