Cancel
Showing results for 
Search instead for 
Did you mean: 

Angled Planes Created From Base Plane

Valued Contributor
Valued Contributor

Confused...  Could someone explain how to create an angled plane based on a base plane that's not rotated 90°?  Not sure what I'm missing.  See below...

 

Capture.JPG

 

Thanks,

 

Matt

2 REPLIES

Re: Angled Planes Created From Base Plane

This is one of those things that you really need to follow the status bar for....

 

In ordered mode I never got good at doing this... though after a few trial and errors and slowing down to follow the status bar dirictives I could get what was needed...

 

I suggest using sync for planes manipulation...  it is just simply so easy it's like cheating...

 

if you can use sync for your plane creation i suggest doing so...

 

see this short video:http://screencast.com/t/1W9R3oU8I

 

Re: Angled Planes Created From Base Plane

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I've always wondered about this too. Oddly if you select the top plane first it keeps the same orientation. Other planes flip 90 for whatever reason. I've always just lived with it. Now using synchronous, which doesn't show that orientation rectangle, I don't concern myself with it.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200