Cancel
Showing results for 
Search instead for 
Did you mean: 

Angles plane

Valued Contributor
Valued Contributor

Hi,

 

I want to create a plane at a 30 degree from the flat top of this part.  The pivot line for the plane is correct, but it's only letting me change the angle between the plane and the slope.

 

plane.png

13 REPLIES 13

Re: Angles plane

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you have to have the XY plane (the pivot) coincident where you show it it seems to me you'd have to know the angle of that slope relative to the top, subtract it from 30 and use the result for the angle from the flat top.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Angles plane

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Also not sure why you care where the "pivot" is. This is one of those cases where this might be easier in sync. At least in terms of getting the angle and getting the plane coincident with that line without needing calculations.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Angles plane

Honored Contributor
Honored Contributor

If you want to stay in ordered. I find creating sketches on the typical planes the easiest first step. then create a plane either with 3 point or normal to curve. The sketch allows you to have control over the plane angle.

Re: Angles plane

PLM World Member Genius PLM World Member Genius
PLM World Member Genius

I have given up using planes (which is probably bad in general) for angled work. I usually use a sketch which I extrude to form a surface. This automatically creates something I can draw on and attach to for assembly purposes, and I don't have to go through the pain of making planes.

Shane Murray
SE2019 MP6
Highlighted

Re: Angles plane

Phenom
Phenom

Create the angled plane to the top surface then create a plane parallel to it, using the front corner of the sloping surface to define the offset distance.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Angles plane

Community Manager Community Manager
Community Manager

Use the Angled Plane command like you were. Select the FLAT plane as the parent. At the step for "Edge to Pivot About" (or whatever it says), pick the vertical end face. It will then create a virtual edge at the intersection of the horizontal and vertical planes and pivot 30 degrees about that. Shoudl be what you are after.

Dan Staples
Director, Solid Edge Product Development

Re: Angles plane

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@dcstaples, except that the pivot will be a virtual line above that shown in the original image.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Angles plane

Community Manager Community Manager
Community Manager

Sure. Then you do a parallel plane through the edge in question if that is important. This is of course the issue in ordered -- you have to have a "recomputable" set of steps and therefore constructs can sometimes be a bit more involved.

 

Dan Staples
Director, Solid Edge Product Development

Re: Angles plane

Honored Contributor
Honored Contributor

When I use angled planes, I typically need to go back and move the pivot point, angle, and position as part of the design cycle. This is why I like a sketch to be in control allowing complete freedom of the planes position without losing at references like includes and parallel relation from the plane. If I picked anything I can't move as the pivot point....I would have to start over. Anything downstream becomes lost.