Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Angles plane

Valued Contributor
Valued Contributor

Thank you for all the suggestion.  When creating angled planes, I wish there was an option to constrain the plane just like a sketch.  I don't know if this is possible, but it would be very helpful if one could dimension the plane angle relative to another plane, geometry, or solid face.

Re: Angles plane

MLombard
Retired

Well, you can't make an angled plane for some reason in Sync, but you can make a planar surface, and put an angle dimension to it. Unfortunately, that turns up as a purple reference only dimension, which can't be changed by the user directly or used in a formula. It can be changed by using the steering wheel to angle the surface body. And there is no angle relation to persist, aside from Perpendicular. So for this, I would again use an ordered plane.

Retired Community Manager for Solid Edge. This account is no longer active.

Re: Angles plane

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"I wish there was an option to constrain the plane just like a sketch"

You can generate a plane using sketches and change the sketch to change the plane. Look at a 3 point sketch or a sketch normal to curve for examples.

In ordered of course.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Angles plane

Gears Phenom Gears Phenom
Gears Phenom

Guys,

 

I know, you are talking about Angles plane, but... In my life I've already met lots of challenges and this "plane story" is interesting a little bit.

I suggest using coordinate system instead of plane, because you have better control above it and you can use three "planes", and etc...

 

Here is a video how it works in this case:

 

BR,

Imics
http://solidedgest.wordpress.com/