Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Annotate Text - counterintuative

Not applicable
So you type a few characters like "abde"
You forgot the c, so you click between the b and d
(well you've just made that text box complete)
So, the program starts typing about halfway down as a new box.

I'm not finished the first box.

Behavior is exagerated when you have a grid and have the background set to Magenta.

Expected behavior, Have a nice box to type in that will resize as you go along.

The interface behaves as expected when you hit enter at least once, but not if it's a single line.
1 REPLY 1

Re: Annotate Text - counterintuative

Not applicable
Ron,
There are two ways to start a text box.
There is single click as you are doing.
This defines a start point for text with no range.
In this case, use the arrows to move within the text.
You can also use click and drag to define a box to type within.
As long as you are manipulating the text within the box,
you can use the mouse to click to place more text.
Regards,
Rick B.
"ron.dozier@gmail.com"

wrote in message
news:ron.doziergmail.com.4y181o@noreply.bbs.industrysoftware.automation.siemens.com...
>
> So you type a few characters like "abde"
> You forgot the c, so you click between the b and d
> (well you've just made that text box complete)
> So, the program starts typing about halfway down as a new box.
>
> I'm not finished the first box.
>
> Behavior is exagerated when you have a grid and have the background set
> to Magenta.
>
> Expected behavior, Have a nice box to type in that will resize as you
> go along.
>
> The interface behaves as expected when you hit enter at least once, but
> not if it's a single line.
>
>
> --
> ron.dozier@gmail.com
> ------------------------------------------------------------------------
> ron.dozier@gmail.com's Profile:
> http://bbs.industrysoftware.automation.siemens.com/vbulletin/member.php?userid=277124
> View this thread:
> http://bbs.industrysoftware.automation.siemens.com/vbulletin/showthread.php?t=46116
>