Annotation part vs. assembly

Honored Contributor
Honored Contributor

I use annotation to call out information in a drawing specific to a part like name or number from a graphic connection.

 

Now what if I want the graphic connection to a sub assembly instead of it's components? what kind of formatting is that, if it's available.

 

Note: the R1 bit will not work, as it could be the 10th or 50th part inserted

4 REPLIES

Re: Annotation part vs. assembly

SeanCresswell 2nd Gear
2nd Gear

It's a manual selection though, as list is populated by what exists on the draft sheet[s] already....but, I would use "Named Reference".....then the selections available.

 

 

ST8_DFT_Callout_PropertyText_NamedReference.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP3] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Annotation part vs. assembly

Phenom
Phenom

Provided the sub-assembly isn't expanded in the parts list, Graphic Connection should give the properties of the sub-assembly.

Graphic Connection to Part will still give individual part properties, regardless of whether the sub-assembly is expanded.

 

I raised the point in another thread that when 'Include Top-Level Assembly in Parts List' is checked, the parts list should give that an item number that can be ballooned etc.

At the moment we have to manually assign balloons for the top level.

HP Z420 16GB RAM
Quadro K4000
ST10 MP3 on Windows 10 Pro 64.

Re: Annotation part vs. assembly

hawcad 3rd Gear
3rd Gear

Hi,


as mentioned the two different methods of graphical connection will do exactly You are looking for.

 

 

%{Filename|G} e.g stands for Graphiocal connection (SubAssembly) while

%{Filename|GP} brings me the Graphical Connection to Part 

 

20151202_1120.PNG

 



regards
Wolfgang

Re: Annotation part vs. assembly

Honored Contributor
Honored Contributor

That was what I could not remember. the |G vs the |GP switches.

 

Many days I can't get at the on line help because of poor on line access. This was the case when I posted the question.

 

thanks all.