Cancel
Showing results for 
Search instead for 
Did you mean: 

Applying Two Angles Together

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I am applying to angles together. 

Both planes line up, one is set up to a wall and the other set on the floor.

I want to combine coming to one another (both angles) 

Angles need to connect together with no offset.

Sorry, my youtube is inop.

 

Thanks

Greg

5 REPLIES 5

Re: Applying Two Angles Together

Gears Phenom Gears Phenom
Gears Phenom

A simple screenshot would help a lot.


____________________________________
--Scott Wertel, P.E.

Betreff: Applying Two Angles Together

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @PO_LC

 

 

 

there is nothing to add to @swertel comment.

 

 

Give us a screen shot to better understand what You are trying to achieve.

 

regards
Wolfgang

Re: Applying Two Angles Together

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor
As so stated, I want to combine the two pins with a deg, angle.
All the ones I've tried can't get to line up.
I hope this helps

Greg

Re: Applying Two Angles Together

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @PO_LC

 

 

which pins, how does they look like, how are they placed, 

 

 

Give as a picture and I'm confident, that somebody here will find a way to do.

 

 

regards
Wolfgang

Re: Applying Two Angles Together

Gears Phenom Gears Phenom
Gears Phenom

when placing an angular dim you need to pay close attention to which angle is being dimensioned; you have 8 choices I believe...   so its possible you are trying to place 2x 45 deg angles but the angle being dimensioned is actually 135 deg?

 

 

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7