Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Arc smoothness with zoom

Valued Contributor
Valued Contributor

Is there a feature to increase the arc smoothness as you zoom in to the curve and the reduce or go back to a set value when you zoom out of the model?

 

 

Regards,

MagRiz
(ST9 User Est 01.18)
3 REPLIES

Re: Arc smoothness with zoom

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @MagRiz,

 

I have the "Sharpness Set" [from the View tab - Style group] in my QAT....to do this very thing. 

 

2018-05-15 (1).PNG

 

It is a long standing [Pet Peeve] request, for the user to be able to set these display quality settings [including Arc Smoothness - in SE-Options] to their highest level, and stay there until the user sets it otherwise.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Arc smoothness with zoom

Creator
Creator

there is also the predefine option where you set it as default , its under the general tab - view

 

Re: Arc smoothness with zoom

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @joorche

 

 

 

the only but big problem herewith is, that after closing SE and starting it new, this setting is set back to a hard default and never is kept from one session to the next.

 

regards
Wolfgang