Cancel
Showing results for 
Search instead for 
Did you mean: 

Area Moment of Inertia

Experimenter
Experimenter

Hello,

 

I'm trying to determine the area moment of inertia of a cross-section of a part.  I'm currently streaming the trial version of ST9; I have been able to find how to do this on older versions of the software on Youtube and other forums, but haven't seen anything for this specifically.  Any help is greatly appreciated.

4 REPLIES

Re: Area Moment of Inertia

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Gguy,

 

In your draft file, go the "Inspect" tab, then under the "Evaluate" group use "Area" command on your section...then once placed, select the area results "Properties", which should have your moment of inertia information.

 

Here is a short video....

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Area Moment of Inertia

Experimenter
Experimenter

Hey @SeanCresswell,

 

That solved the problem for me.  I thought that was where to go, but "Area" was always greyed out.  Turns out I wasn't in a draft file.  Thanks!

Re: Area Moment of Inertia

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Most welcome @Gguy.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Area Moment of Inertia

Phenom
Phenom

You can also do this within the scross-section sketch of a model.

It appears that the values are also added to the variable table - thus they can be exposed in a drawing.

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.