Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly Crashing SolidEdge ST9

Experimenter
Experimenter

Hi guys,

 

For some reason i cant open my assembly after i closed down the programme and reopened it. It just gives me a crash report and closes down SolidEdge. The heavy grey lines are around the draft of the model so im guessing something happened the model.

 

When i go into a new assembly now to start again it crashing again straight away. I can open normal parts and sheet metal parts but cant get the assembly feature to stop crashing... any advice??

 

Sean

2 REPLIES 2

Re: Assembly Crashing SolidEdge ST9

Legend
Legend
1. Enter an IR, record the number.
2. Open the draft in Design Manager, pack and go the whole tree to a zip, rename with the IR number being the start of file name then upload to GTAC.

If you cannot find a Solid Edge setting, confirm you have a file open of the type that will be affected.

Re: Assembly Crashing SolidEdge ST9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Also include your "crashlogf.txt" file found in C:\Users\yourusername\AppData\Local\Temp



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com