09-20-2016 02:37 PM
09-20-2016 02:42 PM
09-21-2016 01:46 AM
Hi,
I think a assembly feature only can take the part colour itself.
The only method I can imagine at the moment is to create the feature in the part and then you can use the part painter to accomplish the different colours
09-21-2016 03:43 PM
09-21-2016 08:38 PM - edited 09-21-2016 08:39 PM
Hi there @TShref,
Does your laser read the PSM directly, or is it based off the "flatten" model.....or a "Save as Flat"?
Reason I ask is, if you were to make the cut at part level [enabling face & feature isolated Part Painter use], you could use "Delete Faces" command to remove it enitrely from the flattened version of the model.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000