Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly File Open..synch

Valued Contributor
Valued Contributor

When you open the part in the assembly it is opened synchronously.
I want to open a traditional ... Do This phenomenon occurs because of what?
ST9 version.
Synchronous is too slow. I do not want to use.

5 REPLIES

Re: Assembly File Open..synch

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Go to Solid Edge App button -> Settings -> Options -> Helpers -> Start... with Synch...

 

Too slow? It depends on... Smiley Wink

 

BR,

Imics
http://solidedgest.wordpress.com/

Betreff: Assembly File Open..synch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


do You talk about an already existing part or a new created part?

 

 

regards
Wolfgang

Re: Assembly File Open..synch

Valued Contributor
Valued Contributor

It occurs when files are opened in the assembly.
Check the Start screen has changed.
...
Synchronous does not move like a unique habitat is cool.
Move slowly.

I always appreciate your answer.

Betreff: Assembly File Open..synch

Valued Contributor
Valued Contributor

Yeah !!
It occurs when you open a File to an existing assembly.

Are you going to be open to the last configuration?

 

 

Re: Assembly File Open..synch

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hi,

When you open parts whether it's in assembly or single part, it's depend on which system were used to create the part (Synchronous/Ordered), you can hide previous level assembly while edit in place and or inactivate all other parts.