Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly JT import as .par

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi Edger´s

 

I want to Import an Assembly JT into a .par Template.

 

But unfortenately the result is an teselated Body feature...

 

In my opinion i should get an multibody Part with two Volume bodys...

 

What am i doing wrong?

 

The funny thing is, if i open this jt with an .asm template i get an .ASM with two parts and they are correct as expected.

 

I also tried some settings in the SePvTrn.ini, "Import Multiple Bodies As Single Part file=On" but for me there was no change in the results...2016-10-25 13_50_33-Solid Edge ST9 - Assembly - [Dateiname].pngASM Template2016-10-25 13_50_09-Solid Edge ST9 - Ordered Part - [Dateiname].pngPAR Template

 

Thanks in advance, see attached the Jt file (I had to ZIP it because .JT is not allowed as attachement...)

 

 

6 REPLIES

Betreff: Assembly JT import as .par

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

 

could it be, that You only exported a rough (triangle)  JT file instead of a fine (B-Spline) .

That could explain the teselated body.

 

There is an option in the export steps to define the quality of export.

 

 



regards
Wolfgang

Betreff: Assembly JT import as .par

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi,

 

yes i know that options, i used the settings ses screenshot (iclude precise geometry)

2016-10-25 15_12_47-Speichern unter.pngJT Options

 

See also my comment in above with the .ASM template.....

 

 

Betreff: Assembly JT import as .par

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,



OK, it seems, that the JT is a fine geometry rather then a coarse.

Importing the JT file into an assembly creates a parts structure which also could be modified.

 

 

At the moment I only see a way to import the asm first and interpart that into a part document.

 



regards
Wolfgang

Betreff: Assembly JT import as .par

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Thanks for the answer,

 

I also tried this before, it works correct, but i just do not understand this behaviour...

 

We have implemented the Multibody technique, so why this is not working on JT Import.

 

Greetings Christian

 

 

Highlighted

Betreff: Assembly JT import as .par

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi,

maybe it is a matter of the translator rather then Solid Edge itself.


regards
Wolfgang

Betreff: Assembly JT import as .par

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello together,

 

i filed an IR, it  was an PR and now it is an ER 867196 with the status OPEN

 

Just for your information, if you have the same Usecase.

 

Regards Christian