Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly Statistics menu to the mouse R button?

Valued Contributor
Valued Contributor

Can I add the Assembly Statistics menu to the mouse R button?
The extension Asm has menus such as report and design manager.
Can I add assembly statistics?

 

How to modify and use the registry?

Mouse R asm.png

 

2 REPLIES

Betreff: Assembly Statistics menu to the mouse R button?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

the Right Mouse Button DropDown Menu already has the function "Assembly Statistic"

20170314_0836.PNG

 

 

 

AFAIK there is no possibility to change the RMB DropDown only the RadialButton, ShortCut, Symbol and Fast Menu

 

 



regards
Wolfgang

Betreff: Assembly Statistics menu to the mouse R button?

Valued Contributor
Valued Contributor

This is not done inside EDGE.
I want to add a menu that comes out by selecting an assembly file from the outside.
Assembly reports can do so.

I wondered if I could add that to assembly statistics as well.
If it is made into a file through a separate API, it seems to be possible.

 

Thank you For Answer.