Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly alignment

Valued Contributor
Valued Contributor

I mated this bolt with the base using the Insert relation.  I unlocked the rotation and can free turn the screwe with the steering wheel.  I want to align a face of the bolt with the side of the base. I should be able to use Planar Align to achieve this, but I get an error saying it conflichs with another relation.

 

I double checked the existing relations for the bolt and there is only an axial align (unlocked rotation) and mate.  Why can't I use planar align to align the bolt face with the side of the base?face1.pngface2.png

6 REPLIES 6

Re: Assembly alignment

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Make sure the planar align is floating, not distance locked.

 

floatalign.JPG

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Assembly alignment

Valued Contributor
Valued Contributor

Man, you're just too quickSmiley Happy

 

I have a follow up that's sorta related.  Whenever I try to mate or planar align two faces, I always get a red offset dimension.  I tried typing zero in the distance box, but it never does anything.  I have to enter the relation with the offset, escape out, select the part again, doubleclick on the mate relation, and then set it to zero.

Re: Assembly alignment

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Are you putting the value in the dim tool bar? (next to my circled area on the last reply?)

IDK, it works for me.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Assembly alignment

Valued Contributor
Valued Contributor

Yes, that's where I put it.

 

face3.png

 

face4.png

 

What I have to do is press escape again, click on the part, double click on the relation, then I can make the offset 0.

Re: Assembly alignment

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is the radio button shown off? Although if it's 0 in the dim box it should override this.

 

dimoffset.JPG

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Assembly alignment

Valued Contributor
Valued Contributor

It is now Smiley Happy

 

Thank you very much.  I'm glad there are experts like you here who know exactly where all these options are.