Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Assembly configurations with assembly features?

Valued Contributor
Valued Contributor

I have an assembly of two boards that are glued together then the ends get mitered.  Each part is modeled cut square and I have an assembly feature to show the miter.  Is there any way to suppress the assembly features in an assembly configuration so i can show the assembly in a draft before and after mitering?

 

I can do it with alternate assemblies, but would prefer to avoid those.

 

Using ST9

 

Thanks,

Brian

 

 

2 REPLIES 2

Re: Assembly configurations with assembly features?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In view properties under model options there's button to hide assembly features. See if that does what you want.

This is in draft by the way.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Assembly configurations with assembly features?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

This is another case where a feature or functionality is available in Draft but not in the assembly itself.

The other one is showing parts transparent without having to create a new facestyle.