Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly drawing dimensioning, balloon sequences and scale migration.

Hi Everyone,

 

I've a few questions regarding to Assembly Drawing. If anyone know how to solve them or know the sources/link to get the solution, hopefully can help me.

 

1) Can Solid Edge retrieve the dimension that already assigned in parts into assembly drawing. For Assembly design can retrieve using retrieve dimension command. How assembly drawing?

 

2) How to customize the sequences of the balloon. How to manipulate the Item Number?

 

3) After finish doing assembly drawing, the file can be save as AutoCAD file (.dwg), but the scale is not maintain to 1:1. How to control the scale?

 

Thank for help.

ST9 Solid Edge user

Windows 10

AutoCAD 2016

 

4 REPLIES 4

Re: Assembly drawing dimensioning, balloon sequences and scale migration.

Gears Phenom Gears Phenom
Gears Phenom

To manipulate item number, you have to go into your parts lists properties, and under the options tab check the box for "Renumber items/balloons according to sort order", then if you go to the sorting tab and for the first sort criteria you set it to "ITEM" then you can click on a part balloon and key in whatever number you wish. If you want something to go to the end of the line and say you have 20 parts, set it to item 21 and the whole list will reorganize with that part at the end of the parts list at item 20.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Betreff: Assembly drawing dimensioning, balloon sequences and scale migration.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Muhammad_Ayub

 

 

 

 

  • You can retrieve dimensions which was set within the assembly (PMI) using PMI display configurations to be retrieved into the ASM drawing

 

 

  • have You walked through the DWG output options before save it?
    Which scale was applied to the DWG?

 

  • the item numbers can be manipulating using the sort order of the BOM, or can be changed manually within the BOM or YOu can do it in the ASM with retrieving the item numbers from the ASM.
    All is done via the BOM option and property form
regards
Wolfgang

Betreff: Assembly drawing dimensioning, balloon sequences and scale migration.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The item number and data tabs in parts list properties can be used as well but make sure no sorting rules are active.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200
Highlighted

Re: Assembly drawing dimensioning, balloon sequences and scale migration.

Phenom
Phenom

When you save as DWG, select options and step thru the translation wizard. On the second page of the wizard you will find the scaling otions. At the end of this process you will need to save the seacad.ini file to a new name as the original seacad.ini cannot be overwritten.

 

 

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317