Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly features (welds)

Gears Phenom Gears Phenom
Gears Phenom

I rarely have assemblies that I create weldments from but I occasionally do. My issue is that besides creating an assembly configuration, you can't select the features (weld beads) and hide them? I have a 6 part assembly with 14 weld beads.. Seems like alot of work to select them all individually! why can't we at least highlight/select them all?  

Anyone create a lot of weldments and deal with this?  

-Craig
2 REPLIES 2

Betreff: Assembly features (welds)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Craig_H

 

 

I would recommend to use the ST9 functionallit of putting weldment bodies into single extra parts.

 

This IMHO brings a lot in perfromance and functionallity as well as ou can do everything what You normally also can do with other parts

 

regards
Wolfgang

Betreff: Assembly features (welds)

Gears Phenom Gears Phenom
Gears Phenom

@hawcad wrote:

Hi @Craig_H

 

 

I would recommend to use the ST9 functionallit of putting weldment bodies into single extra parts.

 

This IMHO brings a lot in perfromance and functionallity as well as ou can do everything what You normally also can do with other parts

 


Ahh yes, Like I said I rarely show welds, I remember now reading about this but never done it, Thanks!

-Craig