Cancel
Showing results for 
Search instead for 
Did you mean: 

Betreff: Assembly holes

Impressive. Many thanks.

I'm starting to like SE.
Tiago

Re: Assembly holes

Gears Phenom Gears Phenom
Gears Phenom

if you use boolean from assembly to a hardware part this should happen for you automatically.   

 

From ST9 Whats New Doc.

 

4-21-2017 8-38-10 AM.png

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Betreff: Assembly holes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

TiagoFigueiredo schrieb:
Impressive. Many thanks.

I'm starting to like SE.

 

 

Hi @TiagoFigueiredo

 

 

welcome and this is the best acknowledgment You can give:

 

"I'm starting to like SE"

 

We already do so!
Smiley Happy

regards
Wolfgang

Betreff: Assembly holes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @TiagoFigueiredo

 

 

by the way, the IMHO best You also can do is to look into the tutorials.

 

Go to the help page of the path finder and walk through the "learning path" and the "Solid Edge Help"

 

20170421_1519.PNG

 

 

If  You download the self-paste tutorials You wil get 1000s of pages with examples and explanations

 

regards
Wolfgang
Highlighted

Betreff: Assembly holes

Honored Contributor
Honored Contributor

I just had a very long talk with a new cad guy I am training yesterday about a related subject. Our conclusion was that the desired results are impossible.

 

What I am looking for is a way to have the hole for an object to be inserted with the object. But here are the obsticles that I think prevent this from ever happening.

 

- the hole needs to be added to sheet metal in a way it shows up in the flat pattern. So assembly features can't be used.

 

- The item associated with the hole will live in the hole. So a process must include the sequence of creating the hole than adding the object

 

- The item is a simple in house created part.

 

The deal breaker is that the operation needs to effect two files. The hole is added to a sheet metal part, but the object to live in the hole needs to be another part in the assembly.

 

So no way to get that done. Does anybody know a work around to create a single step operation to add a hole and object in a single step. If there was a way to do this, then the required hole size for each object to be placed in holes could be saved with the object.

 

As a simple example, I want to place a coupling placed half way through a piece of sheet metal. The hole is oversized 1/16" from the hole.

 

 

Betreff: Assembly holes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @12GAGE

 

 

 

 

good point and what's about a "System Library"?

 

Wouldn't this do exactly You are descibing?

 

20170421_1554.PNG

regards
Wolfgang

Betreff: Assembly holes

Honored Contributor
Honored Contributor

I will give that a look when time is available. Thanks for the suggestion hawcad.

Betreff: Assembly holes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @TiagoFigueiredo

 

 

IMHO = In My Honest Opinion

 

 

@12GAGE

 

Yes I think that can help You for several tasks

 

 

regards
Wolfgang

Betreff: Assembly holes

Honored Contributor
Honored Contributor

I thought IMHO = In my humble opinion.

Betreff: Assembly holes

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @12GAGE

 

 

this is what I also thought but did a search via google which brought "honest"

 

I personally also prefer humble

regards
Wolfgang