Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly mirror out of date

Experimenter
Experimenter

Goodmorning all,

 

I'm having a weird issue in the assembly environment. i have mirrored 2 psm files over the X-Z plane (Rotate). when i finish the feature everything is ok. but when i click on: Update Active Level. a clock occurs in front of the feature and an error screen comes up: Conflicting relationships. 

 

How can i solve this?

 

Knipsel.JPG

Knipsel2.JPG

 

5 REPLIES

Re: Assembly mirror out of date

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @SteelMachines2,

 

Strange....could this be a write access issue?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Assembly mirror out of date

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Pretty hard to tell without having the files. Did you open the original and mirrored part to investigate?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Assembly mirror out of date

Valued Contributor
Valued Contributor

Hello @SteelMachines2,

My same issue solved by following below process.
Please check if you don't have other solutions yet and let me know if it works for you.

1. Right click in 'Mirror' (which is out of date)
2. choose 'Edit Definition' from that menu
3. don't do anything. just save the file from SE application menu and close SE.
4. open the assembly file again, update it. And it should be solved.
5. save the assembly file

Regards,
Aslam

Re: Assembly mirror out of date

Valued Contributor
Valued Contributor

Hello @SteelMachines2,

 

unfortunately the issue comes some times later again!

 

Regards,

Aslam

Re: Assembly mirror out of date

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @aslam

Hi @SteelMachines2

 

 

 

maybe YOu can upoad those files to the forum.

Only then any serious investigatian is possible.

regards
Wolfgang