Cancel
Showing results for 
Search instead for 
Did you mean: 

Assembly problems

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello all,

 

I have encountered a problem while working in a asemmbly. When I move my cursor over sub-assembly in path finder, it hilightes my assembly and showes some extra components in environment. But when I enter that sub-assembly, I cannot see them in it. I dont want these hidden components to be appeared when I move my cursor over assembly. 

I have tried hide/unhide and supress/unsupress option. 

 

Please help me solve this.

 

I have attached a short video and some snapshots of problem.

2 REPLIES

Betreff: Assembly problems

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @3DRohan

 

 

I suppose that without having more information it will be hard to find the reason for that behaviour.

 

First of all: "What version of Se are You using?

 

 

And now let' assume ceratin standard issues.

 

  • What graphic card to You have, and operating system, service pack, graphic card driver?
  • Does the problem occur after closing Solid Edge, open it new and open the assembly again?
  • Will it be also after reboot the compute?
  • And if all the above doesn't occur or doesn't change anything,
    then have taken a look into the occurency properties of the complete structure, wether there are some elements with "not shown on higher level"
  • If this also doesn't be the reason then I think it might be necessary to have this assembly for opening and working to see what else it could be.

 

 

 

regards
Wolfgang

Re: Assembly problems

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello Rohan:

 

Try restarting Solid Edge if the issue is still there.

 

Also try changing the setting in Solid Edge Options - View - Application Display - Graphics Card Driven (Advanced).

 

Hope that helps.

 

Tushar