Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Assistance in experimenting ANSI Draft

Creator
Creator

Respected Sir,

 

I am using solid edge st8 though I actaully wanted st5 version.In st5 we have 'n-sided polygon' option used for drawing pentagons and hexagons but this option is not available in the st8 version.Someone please help me out at the earliest.

 

5 REPLIES

Re: Assistance in experimenting ANSI Draft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It's there in ST8. It is now called "Polygon By Center".  Use Command Finder to locate it.

 

ST8 will have way more features than ST5 because it is newer.  You don't want ST5.

 

 



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Re: Assistance in experimenting ANSI Draft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Student1, we went over these same things in an earlier thread yesterday.

Bruce Shand
ST10 MP10 - Insight - Win10 - K4200

Re: Assistance in experimenting ANSI Draft

Creator
Creator
Yes sir,I know that.I had posted the same questions in two different places to make sure that I get a reply. Thanks a lot for your assistance. It was immensely useful.

Re: Assistance in experimenting ANSI Draft

Creator
Creator

Sir,

Which font style do we get alpha,beta and gamma in ANSI Draft ST8?


@Grundey wrote:

It's there in ST8. It is now called "Polygon By Center".  Use Command Finder to locate it.

 

ST8 will have way more features than ST5 because it is newer.  You don't want ST5.

 

 


 

Re: Assistance in experimenting ANSI Draft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Almost all the Windows fonts have complete character sets.  You will need to use the Character Map tool to see them and then copy them to be able to paste them in your string.  Example "Delta" below:

Δ

 

2016-08-18_12-39-06.png



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com