Cancel
Showing results for 
Search instead for 
Did you mean: 

Associative assembly sketch

Honored Contributor
Honored Contributor

I'm not able to set up a sketch to drive hole patterns that span multiple pieces. Here are the details.

 

Typically, I create sketches with hole patterns within sheet metal parts.

I create cutouts using the sketch.

Other parts are mated to the hole patterns.

To move the other part, I then go adjust the hole pattern.

The hole locations maintain a perpetual relation to the cutouts.

 

Currently, I want to sue the same procedure, but the hole patterns are spanning multiple pieces of sheet metal.

I can get the cutouts in place across multiple pieces using an assembly sketch, and then make assembly driven part features in the sheet metal parts.

The problem is that assembly sketches can't automatically update (Perpetual relation) each piece of sheet metal.

 

Any suggestions?

 

 

3 REPLIES

Re: Associative assembly sketch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Scott,

 

Pretty certain you should be able to do this already......by using "Project to Sketch" with "Maintain associativity..." checked ON, then actually include some geometry on those parts, in order to link it to the pattern sketch. Still only as robust as the edges the geometry is derived from.

 

ST8_ASM_Sketch_ProjectToSketch_PartProjectionOptions.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Associative assembly sketch

Honored Contributor
Honored Contributor

That's the problem. I use thoes options all the time for sketches within a part. But it does not work for an assembly sketch that is to be applied to multiple parts.

Re: Associative assembly sketch

Honored Contributor
Honored Contributor

I figured it out. The way I want to work requires the option: Create Assembly-Driven Part feature vs. Create part feature or Create assembly feature.

 

I had always wondered the differeance.....now I know.