Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Attach dimensions

Builder
Builder
Yes

Re: Attach dimensions

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Not any more. Tried just straight dragging a detached dimension, and holding the ALT key with the same result... Didn't realise there was a button.

 

It also seems that reattaching centrelines has become a problem also. Used to be able to drag the handles in a centre between 2 lines but now, it always shows as between 2 points.

 

If there is any consolation, it would seem that centre marks still can be dragged and reattached. 

Shane Murray
SE2019 MP3

Re: Attach dimensions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hallo,


as mentioned in another thread, both is working here, reattaching using the ALT key as well as the function itself is there.

 

 

regards

Wolfgang

 

regards
Wolfgang