Attribute Editor Macro in imported DWG files

Phenom
Phenom

The attached macro can be used to edit Block Attributes when DWG files are imported into Solid Edge Draft.

 

I wrote this macro to help migrate a reluctant AutoCAD user to Solid Edge who wanted this functionality. A block with attributes from DWG is converted to a group with text boxes in Solid Edge and a Bottom-Up selection mode could do the trick but the user insisted on having a dialog UI similar to that in AutoCAD.

 

Note: This program cannot be used for editing a Block Label in Solid Edge block for it is a completely different animal.

 

Here's a video:

 

 

Download the program.

 

If you find the macro useful, kindly do share your experience and the scenario.

Suggestions to improve the program are welcome.

 

~Tushar Suradkar

www.SurfAndCode.in

 

3 REPLIES

Re: Attribute Editor Macro in imported DWG files

Genius
Genius

Great work on the macro!

 

Does anyone know if a macro exists for opening .dwg files and re-saving them as .dft, I have over 900 .dwg files i'd like to convert to .dft and was kinda hoping there was an automated method to do this?

Re: Attribute Editor Macro in imported DWG files

Siemens Phenom Siemens Phenom
Siemens Phenom

Look at the Batch.exe provided with Solid Edge under "C:\Program Files\Solid Edge ST8\Custom\Batch\Bin"

Re: Attribute Editor Macro in imported DWG files

Genius
Genius
Great thanks!