Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Auto Save annoying feature

Valued Contributor
Valued Contributor

Hi Guys

One thing I find annoying with auto save is that the timer doesn't reset if I do a manual save.

And the prompt to autosave always seems to pop up in the middle of an action.

 Could the auto save prompt be programmed to delay until there is a pause in drawing and reset after a manual save?

 

Cheers

Pete

1 REPLY 1

Re: Auto Save annoying feature

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

AutoSave should already wait for a command to be complete before prompting.

 

I imagine that they could reset the timer based on a manual save but a request to do that would need to be turned in through the proper channel by a customer under maintenance.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com